BRAKE#.AXIS

Description

Sets which axis will control the brake.

Value Description
0 Not used
1 Controlled by Axis 1.
2 Controlled by Axis 2.

Examples

Context

For more information see Brake.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

Depends on Brake and Axis number:

BRAKE1 defaults to 1.

BRAKE2 defaults to 2 on multi-axis drives and 0 on single-axis drives.
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
BRAKE1.AXIS

3012h

01h

Unsigned8

-

-

Read/Write

No

BRAKE2.AXIS

3012h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

BRAKE1.AXIS

3100

C1C

Unsigned8

Read/Write

-

BRAKE2.AXIS

3101

C1D

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

BRAKE1.AXIS

3100

Unsigned8

Read/Write

-

BRAKE2.AXIS

3101

Unsigned8

Read/Write

-